Technical FAQs

Ask a Question

Can the HPALM handle padlock attachment be used to lock the MAL breaker in either the ON or OFF position?

No. The HPALM will lock the MA, MAL, MH, MHL, ME, MEL, MX and MXL circuit breakers in the OFF position only. Where locking in the ON position is required for these breakers, use the HPAXLM padlock attachment and MAHEX handle extension together.

CTA-ID : 2009127
Was this helpful?
What can we do to improve the information ?