Technical FAQs

Ask a Question

What is the maximum main amperage available in a QO load center?

QO load centers are available with mains up to 400 ampere (single phase, NEMA 1), 225 ampere (single phase, NEMA 3R) or 225 ampere (three phase, NEMA 1 or 3R). For higher amperages, consider a NQOD panelboard.

CTA-ID : 2008886
Was this helpful?
What can we do to improve the information ?