Technical FAQs

Ask a Question

Can Versa-Crimp lugs be used on both the line and load side of a safety switch?

Yes, if the switch is suitable for use with Versa-Crimp lugs, they can be applied to both the line side and load side of the switch.


CTA-ID : 2008694
Was this helpful?
What can we do to improve the information ?