Technical FAQs

Ask a Question

Why will the system not allow an order to be placed on chassis ATV66C23N4U drive and directs you to contact Product Management?

This unit is a size 7 chassis and while field services does have the ability to obtain this unit the system directs you to the Product Manager so the order can be cleared through them. The Product Manager wants to be aware of why an order is being placed on a size 7 chassis unit before it is processed.


CTA-ID : 2008692
Was this helpful?
What can we do to improve the information ?