Technical FAQs

Ask a Question

What type of resets are available for Motor Logic overload relays?

The standard is a manual reset and there is a field installable Remote Reset available which can be wired for automatic reset by using timing relays and auxiliary contacts.

CTA-ID : 2009368
Was this helpful?
What can we do to improve the information ?