Technical FAQs

Ask a Question

Will the NALM6 (600A main lug kit) accept aluminium and copper wire?

Issue:
Will the NALM6 (600A main lug kit) accept aluminium and copper wire?

Product Line:
Pre Series E1 NF panelboards and accessories

Environment:
Installation

Cause:
Selection

Resolution:
Yes

September, 2017 update:  The NALM6 main lug kit is obsolete.  The kit was for the pre Series E1 NF panelboard, either Series 0 or no series indicated on the panel.  The lug kit
is obsolete with no replacement.  Replace the entire panel with a current series NF panelboard.    



 
Was this helpful?
What can we do to improve the information ?