Technical FAQs

Ask a Question

Is a connector required to connect a straight length to an elbow in the LDB wireway?

Yes, two adjacent pieces of wireway must be connected using a connector.


CTA-ID : 2009101
Was this helpful?
What can we do to improve the information ?