Technical FAQs

Ask a Question

Are field installable electrical accessories available for the NHL frame breaker?

Issue:
How can he get a shunt trip for a NHL261200?

Product Line:
Molded Case Circuit Breakers

Environment:
NH/NHL frame breakers

Cause:
Accessories

Resolution:
There are no field installable shunt trips, aux contacts, or any other electrical accessory available for the NH/NHL frame breakers. This was a completely different frame type from the NA/NAL frame breakers, which did have field installable electrical accessories available, depending on when the breaker was manufactured.

The NHL breaker is now completely obsolete.
Was this helpful?
What can we do to improve the information ?