Technical FAQs

Ask a Question

On an EZM 3 phase meter center, What are the meter bus/connections?

If the aic rating is 18k or less there is a choice of plug in or bolt on meter connections. If 18k or more, only bolt on type is available. In either case you need to verify selection with the local utility.

CTA-ID : 2009349
Was this helpful?
What can we do to improve the information ?