Technical FAQs

Ask a Question

Can a a Q2M2200MT be made from a Q2L2200 ?

No. The Q2M has studs on one end. Terminations on the Q2 type breakers are factory-installed only, and cannot be modified in the field.

CTA-ID : 2009339
Was this helpful?
What can we do to improve the information ?