Technical FAQs

Ask a Question

What does the ``S`` designate on XUB sensors?

The XUB is obsolete. The ``S`` designated side sensing and we now call it 90 degree sensing with suffix W, so that a typical replacement might be XU8M18MA230W. Be aware that cross reference material may alternately list the new device without the W suffix, but then will include a mirror as a separate part number. Many of these mirrors are obsolete or not readily available. In this case, substitute the product with W suffix.

CTA-ID : 2009086
Was this helpful?
What can we do to improve the information ?