Technical FAQs

Ask a Question

Where is the condition of sale on the internet?

Issue:
Where is the condition of sale on the internet?
Product Line:
Schneider Electric Conditions of Sale
Environment:
Schneider Electric Conditions of Sale
Cause:
Application is calling for documentation stating Conditions of Sale
Resolution:        
Conditions of sale is stated in the back on the 176 Digest right in-front of the index section. Or can be found on http://static.schneider-electric.us/docs/Advanced%20Products/0100PL0041.pdf
 
Was this helpful?
What can we do to improve the information ?