Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a QO200TR, Series G3, enclosed molded case switch?

This device is supplied with a two terminal ground bar factory installed. Each terminal can terminate (1) #14 - 4 AWG aluminum or copper grounding conductor.

CTA-ID : 2008865
Was this helpful?
What can we do to improve the information ?