Technical FAQs

Ask a Question

What is the difference between the A, B & C codes on the 2510 Type K devices?

Pilot light application voltage.

On Two Pole Devices:
A = 115 Vac
B = 230 Vac

On Three Pole Devices:
B = 208/277 Vac
C = 440/600 Vac


CTA-ID : 2004634
Was this helpful?
What can we do to improve the information ?