Technical FAQs

Ask a Question

Where are the bus options in the Medium Voltage Metal Enclosed Product Selector?

Medium Voltage Metal Enclosed Product Selector

600 & 1200 amp bus, aluminum and copper, is in the Product Selector. See dropdown menu for what is standard for each product. Again, there are three products in this selector each with different bus standards. Insulated bus and bus penetration barriers are found under Bus Options.


CTA-ID : 2009334
Was this helpful?
What can we do to improve the information ?