Technical FAQs

Ask a Question

How can the speed reference be adjusted with an Altivar 58 if there is no external reference or speed potentiometer used?

Adjust the low speed (LSP) parameter in menu 2 (SEt).

This changes the speed because with no speed reference signal present, the drive runs at low speed if there is a valid run command. On a new drive the LSP value is 0.

CTA-ID : 2008686
Was this helpful?
What can we do to improve the information ?