Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a L221N, Series E02, safety switch?

Two ground screws are provided factory installed. Each ground screw can terminate (1) #14 - 10 AWG copper or (1) #12 - 8 AWG aluminum grounding conductor.

CTA-ID : 2008859
Was this helpful?
What can we do to improve the information ?