Technical FAQs

Ask a Question

What is the difference between the CU12L400L, CU12L400N and the CU12L400B?

The CU12L400L is a ringless type with a lever bypass. The CU12L400N is a ring type with no bypass. The CU12L400B is a ring type with test block bypass.

CTA-ID : 2009314
Was this helpful?
What can we do to improve the information ?