Technical FAQs

Ask a Question

Where is the date code located on Altivar drives?

The label is located on the right side of the drive and in the lower right corner there is a 4 digit date code.
Example: 9831 is mfg. date of 31st week of 1998.
This is similar of ATV16, ATV18, ATV11, ATV28, ATV31, ATV58, ATV56, ATV66, ATV61 and ATV71 drives.
It is also part of the serial number for the drives. The date code normally follows the first two digits.

CTA-ID : 2009306
Was this helpful?
What can we do to improve the information ?