Technical FAQs

Ask a Question

What do the 9038 Type BG float Rod lever Figure Numbers 1, 2 and 3 mean? On page 20-26 Digest 172.

These pertain to the float movement:
1 Horizontally mounted, above and below centerline.
2 horizontally mounted, reduced travel
3 Vertically mounted.
This information is located on page 53 of the 9034CT9701


CTA-ID : 2009303
Was this helpful?
What can we do to improve the information ?