Technical FAQs

Ask a Question

What material is in the 9001 TS?

Base and switchknob - Chrome plated zinc alloy die casting , Shaft - Stainless steel, Cam - Zinc alloy, Color inserts - Nylon, Ball Bearing -Stainless Steel, Ball bearing spring - Stainless Steel, Screw and lock washer - Zinc plated steel, Circlip - Spring steel with black phosphate finish, Guide and spacer - Zinc plated steel (sping return type), Seal - Buna N rubber (spring return type), Various pins - Brass or zinc plated steel (spring return type)

CTA-ID : 2009291
Was this helpful?
What can we do to improve the information ?