Technical FAQs

Ask a Question

What is the part number for the replacement 360 VAC coil for an LC1F185?

We do not have a 360 VAC coil but we do have the 380 VAC coil which is LX1FG380 for 50 Hz, LX1FG316 for 60 Hz, and LX9FG380 for 40 - 400 Hz.


CTA-ID : 2009035
Was this helpful?
What can we do to improve the information ?