Technical FAQs

Ask a Question

Are there any standards other than UL1699 to which that the AFCI is type tested to or manufactured?

It provides circuit protection per UL 489.


CTA-ID : 2008815
Was this helpful?
What can we do to improve the information ?