Technical FAQs

Ask a Question

Do you have AFCIs for use in 220V 50Hz single phase applications? If yes, are they UL listed?

No. Max voltage is 120 to ground


CTA-ID : 2008814
Was this helpful?
What can we do to improve the information ?