Technical FAQs

Ask a Question

What rating does adding the protective power terminal covers to the larger units above ...C14Y to ...C32Y provide for the ATS48 because want to mount on wall with just covers?

The power terminal covers LA9F702 and LA9F702 when used on the larger soft starter do not change the rating from IP00 (open) style.  The covers when used and observed properly do help prevent touching of the terminals but the rating is still open style.  The user needs to follow all applicable codes for mounting on wall and in enclosure to obtain desired ratings other than IP00 (open)

CTA-ID : 2009028
Was this helpful?
What can we do to improve the information ?