Technical FAQs

Ask a Question

What is the CFM of the ATV18 fan?

Issue: What is the CFM of the ATV18 fan?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: We do not have this information listed due to the fact that unit was viewed as non-replaceable and non-repairable unit.
The fan is made by Panaflo ( Panasonic ) model number FBK-04F24U rated for 24vdc at 0.16A and an end user can call ( 800-833-3557 ) to order the fan.
The distributor is ( Arrow electronics )



 
Was this helpful?
What can we do to improve the information ?