Technical FAQs

Ask a Question

What are the contact ratings of the 9001 BW pendant stations?

For AC up to 600 volts AC, NEMA B600, 5 amps continuous, make 3600 VA, and break 360 VA. For DC up to 600 volts DC, NEMA P600, 5 amps continuous.

CTA-ID : 2009018
Was this helpful?
What can we do to improve the information ?