Technical FAQs

Ask a Question

What is the heat sink fan part number for an ATV66D12M2U , ATV66D16M2U , ATV66D16N4U and ATV66D23N4U AC drive?


It is the heatsink fan located in the bottom of the drive.

The part # is listed on page 98 (page 104 in Adobe Acrobat) in the VD0C06S304E Receiving, Installation and Sart Up manual in Appendix A - Spare parts list.  The part # for the cooling fans of the other size units is also listed in this table.

CTA-ID : 2005923
Was this helpful?
What can we do to improve the information ?