Technical FAQs

Ask a Question

What is the current rating of the 9421 Type N auxiliary contacts?

The electrical ratings are as follows:

AC Make Break Max. Continuous
120VAC 60A 6.0A 10A
240VAC 30A 3.0A 10A
480VAC 15A 1.5A 10A
600VAC 12A 1.2A 10A

DC
125VDC 1.10A
250VDC 0.55A
301-600VDC 0.20A


CTA-ID : 2008805
Was this helpful?
What can we do to improve the information ?