Technical FAQs

Ask a Question

How can you determine the firmware version of the keypad for the ATV66 unit?

The firmware of the keypad can be located on the back of that device. On the back of keypad toward the top you will see a white sticker with a bar code with numbers above and below. Below the bar code you will find the version of the keypad in the second set of numbers that is printed and it is preceded by a letter V.
Note: if this question comes up because there is a need to replace the keypad it is most important to determine the revision level for the control basket. See resolution 785.

CTA-ID : 2008803
Was this helpful?
What can we do to improve the information ?