Technical FAQs

Ask a Question

How can you determine the firmware version of the control basket for the ATV11 unit?

On the side of the ATV11 unit on the heatsink there is a sticker with the unit part number, bar code and other specifications on it and right below the part number at top of sticker the version of the unit is printed.


CTA-ID : 2008801
Was this helpful?
What can we do to improve the information ?