Technical FAQs

Ask a Question

How can the version of firmware used in an Altivar 58 drive be determined?

Look on the main control board in the section that is raised where the keypad connection is made.
With the keypad removed there is a white sticker mounted on board above the DB9 connector.
This sticker has a bar code and some numbers above and below it.
The numbers located below and to the Right are the revision numbers. They follow the letter V.
Example. V5.3 IE 43


CTA-ID : 2008800
Was this helpful?
What can we do to improve the information ?