Technical FAQs

Ask a Question

Where are the A1, B1, and C1 connections on the smaller Altistart ATS46?

Only the soft starters above 30hp have the A1 (A2), B1 (B2), C3 (C3) have the shorting contactor terminal locations.  

The units ATS46D17N, ... D22N, ... D32N & ... D38 do not have these terminal points.


CTA-ID : 2009009
Was this helpful?
What can we do to improve the information ?