Technical FAQs

Ask a Question

What is the part number for the test normal switch on the 8839 Econo Flex 58 unit?

Two-position selector switch ZB5AD2
Mounting collar with 1 N.O. Contact Block ZB5AZ009
Additional 2 N.C. Contact Block ZBE204
Additional 1 N.O. Contact Block ZBE101
Engraved Legend Test-Normal 65170-166-72
Legend plate holder ZBZ32

CTA-ID : 2008798
Was this helpful?
What can we do to improve the information ?