Technical FAQs

Ask a Question

Is the key switch in the 9001 KY or KZC security stations maintained or momentary?

It is momentary. It is a 3 position spring return both sides to center. It is not available maintained.

CTA-ID : 13505
Was this helpful?
What can we do to improve the information ?