Technical FAQs

Ask a Question

What is the VA rating of a 9001KM transformer light module?

Issue:
What is the VA rating of a 9001KM transformer light module?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
9001 KM2 110-120 volt 25-30 hertz      2.2 VA
9001 KM1 110-120 volt 50-60 hertz      2.4 VA
9001 KM3 208-220 volt 50-60 hertz      2.5 VA
9001 KM4 220-240 volt 25-30 hertz      2.2 VA
9001 KM7 220-240 volt 50-60 hertz      2.0 VA
9001 KM8 277 volt 50-60 hertz             2.4 VA
9001 KM5 380-480 volt 50-60 hertz      2.8 VA
9001 KM6 550-600 volt 50-60 hertz      2.5 VA



CTA-ID : 2007989
Was this helpful?
What can we do to improve the information ?