Technical FAQs

Ask a Question

QD---Have an application for 480Vac. Is there a rating on the QD for 480V?

No, 240Vac is the maximum.


CTA-ID : 2009244
Was this helpful?
What can we do to improve the information ?