Technical FAQs

Ask a Question

What is the amps per square inch rating of our standard copper bus panelboards?

Interior bussing is rated according to heat rise testing. Current Density Rated bus can be chosen in Product Selectors.

Revised 3/10/04

CTA-ID : 2008611
Was this helpful?
What can we do to improve the information ?