Technical FAQs

Ask a Question

What is the ``P`` mean that is shown on the on the long-time, short-time, and instantaneous trip adjustments on the Micrologic breakers (ex.: LE, LX, ME, MX, PE, PX, etc.) ?

``P`` is the product of sensor size times rating plug. It is the ampere value that LSI pickup dials are a multiple of.


CTA-ID : 2008607
Was this helpful?
What can we do to improve the information ?