Technical FAQs

Ask a Question

Can the QOM2200VH main circuit breaker in a SC3040M200F or SC3040M200S be replaced with an alternate ampacity main circuit breaker?

Issue:
Application

Product Line:
CSED

Environment:
Application

Cause:
Verification

Resolution:
This device is marked ``MAINS 200A MAX. SEE SERVICE DISCONNECT FOR RATING``. The main QOM2 frame circuit breaker can be replaced by any QOM2 frame circuit breaker rated from 100 to 200 ampere.


CTA-ID : 2008154
Was this helpful?
What can we do to improve the information ?