Technical FAQs

Ask a Question

What wire sizes will the lugs on the 9065SS410 or 9065SS420 accept?

One cable per phase; 8 awg minimum, 250 MCM maximum.
60 or 75 degree C solid or stranded copper conductors, torque to 200 lb.-in.

CTA-ID : 2004154
Was this helpful?
What can we do to improve the information ?