Technical FAQs

Ask a Question

How much memory does the P and H trip unit have?

The P and H trip units will store a combined total of 100 trips and alarms. 10 of each are viewable from the trip unit screen, 100 combined total viewable through the communications network like Powerlogic. None of the data is lost if the trip unit loses power.


CTA-ID : 2008140
Was this helpful?
What can we do to improve the information ?