Technical FAQs

Ask a Question

Can the QOU be factory ordered with OOUEC quick-connectors on both ends?

No. The reason is that the QOUEC is never to be used on the LINE end. If it were, the wires could easily pull out during a short circuit, resulting in live wires being unrestrained. When it is sold with QOUEC on the ON end, it is understood that the ON end is being used as the LOAD end.

CTA-ID : 2008578
Was this helpful?
What can we do to improve the information ?