Technical FAQs

Ask a Question

What are the replacment lugs for a H365, Series E1 safety switch?

Old Design repair parts

Product Line:
Heavy Duty Safety Switches

Main Lugs


Use 4025113650. This lug will be different from the standard lug(s) supplied on the Series E1 switch, which are obsolete and no longer available. The Series E1 design provided, per phase, one large lug (for terminating 750 kcmil) and one small lug (for terminating 300 kcmil). The 4025113650 (used on a Series E2 equivalent switch) will terminate either (1) #1/0 AWG - 750 kcmil or (2) #1/0 - 300 kcmil.

CTA-ID : 2008089
Was this helpful?
What can we do to improve the information ?