Technical FAQs

Ask a Question

Does the box size change when a TVSS unit is installed on a 600A M/B I-Line panel?

I-Line TVSS units are branch mounted and require 13.5`` of branch mounting space. (They cannot be installed on HCN interiors.)

Revised 3/10/04

CTA-ID : 2007914
Was this helpful?
What can we do to improve the information ?