Technical FAQs

Ask a Question

Is the XY2CE cable pull available in a NEMA 7/9 enclosure?

No. It is designed ONLY for a NEMA 1, 4, and 12 applications. For IEC information see Digest 172, p 23-2.

CTA-ID : 2007910
Was this helpful?
What can we do to improve the information ?