Technical FAQs

Ask a Question

What UL Standards and File number are the MP Meter-Pak meter centers tested and listed under?

Testing and listing of EZM products

Product Line:
EZM Metering

UL Standards and Listing 

Customer request

The MP Meter-Pak meter centers are tested in accordance with standard UL 67, ``Standard for Safety - Panelboards``. Additional UL standards may be referenced within UL 67 for compliance to that standard. The MP Meter-Pak is listed under the UL File E6294.

CTA-ID : 2008575
Was this helpful?
What can we do to improve the information ?