Technical FAQs

Ask a Question

What UL standards and File number are the QO load centers tested and listed under?

Codes and Standards

Product Line:
Homeline Load Centers

Listing and testing

Customer approvals

The QO load centers are tested to UL 67, "Standard for Safety - Panelboards". Additional UL standards may be referenced within UL 67 for compliance to that standard. Also, the QO load centers are listed in UL File E6294.

CTA-ID : 2008574
Was this helpful?
What can we do to improve the information ?