Technical FAQs

Ask a Question

What replaces an MM circuit breaker installed in an NMM panelboard?

There is no replacement for an MM circuit breaker which can also install in an existing NMM panelboard. The NMM panelboard was made from 1933 - 1948, and it is obsolete. Replace the panelboard and its breakers with an NQOD panelboard.


CTA-ID : 2008568
Was this helpful?
What can we do to improve the information ?