Technical FAQs

Ask a Question

Can a shunt trip accessory be added to an EZM11200CBU?

Yes. The main breaker used is the MHF221200. The MA11021 shunt trip accessory can be field installed into the circuit breaker. This shunt trip module is suitable for 120, 208 or 240 Vac. Other shunt trip modules available are MA11042 (24 Vac), MA11037 (277 or 480 Vac), MA11027 (24 Vdc), MA11028 (48 Vdc), MA11029 (125 Vdc) and MA11030 (250 Vdc).


CTA-ID : 2007893
Was this helpful?
What can we do to improve the information ?